Hi team
My customer requires an IC that can output the following signals:
- Sequence -
1. When the input signal changes from high to low, the output changes from high to low.
2. Even if the input signal does not return to high, the output signal must return to high after a certain period of time.
3 . Reset time(t_reset) is fixed type or can be set by external.
If you have any IC or solution that meets the above conditions, please recommend it.
Thank you