Hi team,
Below is the schematic of the CDCLVC1310.
But customer test the XIN pin and get below wave:
Can you help to comment what's the cause of the issue?
is it because the cap input value or maybe the PCB layout?
Lacey
Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Below is the schematic of the CDCLVC1310.
But customer test the XIN pin and get below wave:
Can you help to comment what's the cause of the issue?
is it because the cap input value or maybe the PCB layout?
Lacey
Thanks a lot!
Hi Alan,
Thanks so much for your reply!
Below is my inputs:
1. The spike happened with possibility when the device power on. It doesn't have the specific period.
2. This spike don't affect the output signal
3. The specs of the XTAL is as below:
4. They have add the bypass cap in the VDDO and VDD.
5. they select the mode to be 01 as the XTAL or override mode.
Should the customer change the mode to XTAL bypass mode?
The point to choose the XTAL override mode or bypass mode is just the max voltage of the XTAL output?
If the voltage is larger than 2V, then we need to choose the XTAL bypass mode. right?
Any circuit design difference need to be done between the XTAL bypass mode and the XTAL override mode?
Lacey
Thanks a lot!