Part Number: LMK03328
Other Parts Discussed in Thread: CODELOADER, , USB2ANY, TICSPRO-SW
Hi team,
Please allow me to ask you some questions from our customer as below,
1.
We can see the description in the datasheet as below,
(P.47 - 48 in the datasheet of LMK03328)
-> Outputs 0 and 1 share an output supply (VDDO_01), as well as outputs 2 and 3 (VDDO_23). Outputs 4, 5, 6, and 7 have individual output supplies (VDDO_4, VDDO_5, VDDO_6, VDDO_7). Each output supply can be independently set to 1.8 V, 2.5 V, or 3.3 V. When a particular output is desired to be disabled, the bits [5:0] in the corresponding output control register (R31, R32, R34, R35, R37, R39, R41, or R43) should be set to 0x00. If any of outputs 4, 5, 6, and 7 and their output dividers are disabled; their corresponding supplies can be connected to GND.
I understand that VDDO_23 can be connected to GND when output 2&3 are disabled, is it correct?
2.
Could you advise me the treatment of SECREF_P/_N in the case of non-used secondary reference clock.?
3.
Is LMK03328EVM supported by both CodeLoader and TICSPRO vis USB2ANY?
Best regards,
Satoshi