This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: Timing requirements between SPI_LE and Powerdown

Part Number: CDCE62005

Hi,everyone

According to the document: SPI_LE has to be logic "1 " before the Power_Down pin toggles low-to-high in order for the EEPROM to load properly.

so,(1)Is there a minimum time requirement between SPI_LE and power_down?

       (2)SPI_LE and power_down to be logic "1 " at the same time,OK?

Thanks.