Part Number: LMK04821
Other Parts Discussed in Thread: AFE58JD18
Looking at the output of the LMK04821 SDCLKout using a differential probe (10:1) I can see the following.
The DCLKout outputs look ok, with a nice waveform. The SDCLKout outputs that are providing the 16.6MHz sysref
look "terrible". Is there something I should set differently?
At the outputs of the LMK04821 we have placed 560R shunts, then AC-coupled to the destination and have a 100R termination there (which is actually the sysref input of the AFE58JD18).
Any idea?
Kind Regards,
Ed