one shot mode::
1. Is the programmed time interval still selected as shown in 8.5.3?Or a fixed value?
2. In this mode, if the DELAY/M_DRV pin is connected to the power supply through the closed switch during the power-on period, it is always HIGH. How is the programmed time interval calculated?
3. During power on, the DELAY/M_DRV pin is connected to the power supply through the open switch, that is, the pin is normally connected to R_EXT. After the RESISTANCE READING is completed, the DELAY/M_DRV pin is connected to the power supply through the closed switch, that is, it is always HIGH.
4. Can the DRV respond to the DELAY/M_DRV pin level falling edge?
5. What is the power supply voltage range of this chip?What happens when the supply falls below or jumps around the lower voltage limit?