Part Number: CDCE6214
Hello support team,
We are researching zero delay buffer with level shifter.
I can found zero delay mode in CDCE6214.
Is it possible to do with CDCE6214?
* Clock rate : 148MHz
* Input : 3.3V
* Output : 1.8V
* Propagation delay : zero (please let me know the min/max value)
If you have any alternative options, please let me know.
Best Regards
Hirokazu Takahashi