• TLC555: Body marking and lot size indicator

    Part Number: TLC555

    Tool/software:

    Hi TI team,

    Can u help me how to indicate the lot size and any code show below body marking for TLC 555?

  • TLC555-Q1: Using TLC555-Q1 as a latch

    Part Number: TLC555-Q1
    Other Parts Discussed in Thread: TLC555

    Tool/software:

    Hello, 

    I am planning on using TLC555-Q1 as a latch by just leaving both Threshold and Discharge pins floating:

    The thinking behind is that once the input is low, we need…

  • TLC555-Q1: TLC555-Q1 - Monostable timer

    Part Number: TLC555-Q1
    Other Parts Discussed in Thread: TLC555

    Tool/software:

    Dear Team,

    555 is used for monostable timer.

    After triggered 555, a timer work on MC  and measure time.

    1- TL55Q 26M AJQHG4

    2- TL55Q 87K A2QTQ4

    There is two different 555 chip…

  • TLC555: Simulation result different with calculation

    Part Number: TLC555

    Tool/software:

    Hi team,

    I need a simple circuit to generate a PWM of 1HZ, duty 50%, to drive electro-magnet.

    I downlaoded Tina file on link https://www.ti.com/lit/tsc/slfm002, and modified R2/R3/C1.

    but looks Simualtion and Calcuation…

  • Clock & timing forum

    Part Number: TLC555

    Tool/software:

    I'd like to know if you lot code gets special meaning on last three letters for reference TLC555IDR.

    We longly used lot with end "WDH", recently we see lot with end"ML4", does these letters means something for…

  • TLC555: TLC555

    Part Number: TLC555

    Tool/software:

    I'd like to know if you lot code gets special meaning on last three letters for reference TLC555IDR.

    We longly used lot with end "WDH", recently we see lot with end"ML4", does these letters means something for…

  • NE556: NE556 pulse width detector triggering one shot

    Other Parts Discussed in Thread: NE556, TLC555, NA555

    Tool/software:

    My apologies if I'm posting in the wrong category, nothing jumped out at me as being the "correct" category.

    I have an application with an air pressure pulse being read…

  • TLC555: TLC555CP

    Part Number: TLC555

    Tool/software:

    I HAVE BOUGHT 2800 PCS. DIRECTLY FROM TEXAS WEB SITE, AND WE HAVE SOLDERABILITY PROBLEMS

  • LMC555: Trouble simulating LMC555 (TLC555_6) in PSpice and LTSpice

    Part Number: LMC555
    Other Parts Discussed in Thread: TLC555, PSPICE-FOR-TI, CSD, TINA-TI

    Tool/software:

    Hi TI team,

    I'm having trouble simulating LMC555 (TLC555_6) in LTSpice and PSpice. 

    First is the LTSpice on a Mac OS. I have a very simple Astable…

  • LMC555: Spice model for power, stability and input impedance

    Part Number: LMC555
    Other Parts Discussed in Thread: TLC555

    Tool/software:

    Hi TI team,

    I'm looking for the LMC555 Spice model for power, stability and input impedance study. Where can I find this model? Thanks. 

  • TLC555: PCN change due to factory transfer

    Part Number: TLC555

    Tool/software:

    Hi,

    I have a question about the PCN of TLC555QDR.

    ・Model name: TLC555QDR (www.ti.com/.../TLC555)
    ・PCN: 20231130002.1

    It seems that there are changes in electrical characteristics, etc. in ICs before and after the PCN…

  • TLC555: Maximum Allowable power

    Part Number: TLC555

    Tool/software:

    What is the maxum allowable power for the IC timer TLC555QD

  • TLC555: RESET input

    Part Number: TLC555

    Tool/software:

    Hi Team,

    Reset input of timer 

    0.3V to 1.8V is considered as reset active low?

    greater that 1.8V input is out of reset?

    Kindly confirm.

    Regards,

    Vidhya

  • TLC555: TLC555

    Part Number: TLC555

    Tool/software:

    Hi Team,

    Does output pin need a pull up?

    Thanks,

    Vidhya

  • TLC555: Please advise alternative source of TLC555CP/ TEXASINSTR/ GES40094484-LF

    Part Number: TLC555

    Tool/software:

    Hi TI Team,

    The material TLC555CP is EOL, please provide the alternative source and quote it, thanks.

    Jabil part number: GES40094484-LF

    MPN: TLC555CP

    MFG: TEXASINSTR

  • TLC555-Q1: I want to know supply current (Icc) of TLC555QDRQ1

    Part Number: TLC555-Q1
    Other Parts Discussed in Thread: TLC555, , TLC3555-Q1

    Tool/software:

    Hello, I'm calculating the current consumption for the power supply connected to VCC of TLC555.

    Looking at the TLC555 datasheet, it shows Icc is 700uA at…

  • LMK6C: for 50khz frequency

    Part Number: LMK6C
    Other Parts Discussed in Thread: TLC555

    Tool/software:

    Hi,

    May I know there have Oscillator product can provide 50khz?

    We may find LTC6907 alternative but seems TI product are support over 1Mhz.

    https://www.analog.com/media/en/technical…

  • TLC555: Is TLC555_6.LIB spice file encrypted?

    Part Number: TLC555
    Other Parts Discussed in Thread: TLC556

    Tool/software:

    Is "TLC555_6.lib" spice file encrypted?

    I placed the contents of TLC555_6.lib into QSpice part.

    But now I'm getting missing nodes error.

    It looks ok and uses .SUBCKT…

  • TLC555-Q1: Questions about TLC555 timer operating conditions

    Part Number: TLC555-Q1
    Other Parts Discussed in Thread: TLC555

    Tool/software:

    I designed a circuit using a TLC555 timer. Trigger input connect 5V(fault detect signal)

    -> When a fault occurs (5V->0), a trigger is generated, and when FLT is restored (0…

  • TLC555-Q1: EVM

    Part Number: TLC555-Q1
    Other Parts Discussed in Thread: TLC3555-Q1, , TLC555

    Tool/software:

    Hi,

    My costumer is asking for an EVM for this device for evaluation.

    I see that there is no EVM available for this device but there is one EVM for the TLC3555…

  • TLC555: his simulation file can only simulate 0-400 us,because of TLC555

    Part Number: TLC555

    Tool/software:

     final -20241119-4.TSC

    This simulation file can only simulate 0-400 us, and an error message of U12 occurs when more time is added. What is the problem? How can it be solved so that the simulation can be extended to…

  • TLC555: PCN2023

    Part Number: TLC555

    Tool/software:

    Hi,

    May I know there have any marking change in 2023PCN?

    Is it still the same with below marking before PCN? 

    Thanks!

    Jeff

  • TPL5010: Will this give an 8 hour delays?

    Part Number: TPL5010
    Other Parts Discussed in Thread: SN74HCS164, TLC555

    Tool/software:

    4 pins of TPL5010 used (red boxes). CLR input will be high (pull up resistor and high Z GPIO port) at VDD (2V to 5.5V) power up (so resistor can be read) and will…

  • TLC555 or TPL5010: reference design for 8 hours waiting

    Part Number: TLC555
    Other Parts Discussed in Thread: TPL5100, TPL5000, TPL5010, SN74LV163A, SN74HCS164, CD74HC4060, SN74LV8154

    Tool/software:

    Hi,

    Could you provide reference design to get trigger signal after 8 hours?

    MCU will give the signal to timer…

  • NE555: NE555 Ripple Detector Simulation in LTspice

    Part Number: NE555
    Other Parts Discussed in Thread: TINA-TI, OPA192, TLC555

    Tool/software:

    Dear Team,

    I am working on a ripple detector and timer circuit using two NE555 ICs. My goal is to activate a relay when the ripple lasts for more than 2 seconds…

1 2 3 4 5 »