This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am getting the same issue tried on 3 different machine. I also installed the NI runtime 2024.
Thanks,
Sophin Soeurn
Hi Sophin,
Can you share a screenshot of the exact error you are getting?
The correct labview runtime is:
The labview runtime engine should install as part of the GUI installer. Can you make sure to run as administrator during the install? Can you also make sure there are no firewalls enabled that could be blocking portions of the install?
Best,
Katlynne Jones
Can you also make sure the two dll files shown here are showing up in your install directory?
Best,
Katlynne Jones
Hi Katlynne,
Here is the screenshot. it seem the installer is not correctly installing the labview runtime engine. I'll try to directly download the runtime with the correct version.
Thanks,
Sophin