This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am new with MSDI & trying to interface TIC12400Q1 EVM SPI Communication with External Microcontroller(NXP: S32K118)
So i am transmitting 0x02000000 (DEVICE_ID) and trying to read but i am Receiving 0xe0000003 (POR, SPI FAIL, PARITY FAIL).
With GUI everything working fine bit with external microcontroller i am not able to read even the SPI.
Is there any specific Jumper setting i am missing?
For connection i am referring below mention link.
Hi Salim,
The settings in the link you referenced should work.
Can you confirm the connections and jumper settings you are using, or provide a picture of your board and jumper settings and cables that I can review? Perhaps there is something you have overlooked.
Do you have the USB cable connected when you have the external MCU connected, or are you using an external supply for the TIC12400 VDD?
Can you provide any scope plots of the SPI signals? Using an external MCU for the SPI connections can result in reflections and noise on the SPI signals which could result in bit errors. There could also be a timing or protocol error that is resulting in the SPI communication errors.
Examples of a protocol error are:
If you can provide details of your configuration and scope plots of your SPI communication, I can review it for errors.
Regards,
Jonathan
Hi Jonathan
thanks & appreciate your support.
SPI Configuration : 500000Hz, CPOL =0, CPHA =0.
Do we have to follow any specific mode of SPI?
I am not connecting board with USB. I have removed J7 jumper and e connected VCC(3.3V) from my board to pin2 of the jumper J7.
I have verified the 3.3V connected to J7(Pin-2)
Below Waveform when Jumper J7 Connected in-between Pin1 &2 (No USB cable connected)
C1: CS
C2: Clock
C3 : MOSI
C4: MISO
Below Waveform when Jumper J7 Removed & ExternalMicro_VCC_3.3V Connected to J7-Pin_2 ((No USB cable connected)
Board Jumper connection Picture
SPI PIN Connections:
What i see from waveforms, the level of MOSI & MISO lines is not as expected.
While referring the below schematic i have connected VDD with 3.3V (From External microcontroller)
Hi Salim,
Thanks for the pictures and waveforms, they are helpful. I have noticed a couple of things.
The MOSI and MISO signal lines are not full amplitude. You have also noticed this.
However, for the SPI signal waveforms, I noticed the SCLK polarity is incorrect. The SCLK needs to be LOW when the CS pin transitions and to ensure there are the correct number of falling edges for the data. This is described in the SPI Interface Bus section of the datasheet. I can see a similar MISO waveform with no valid data response from the TIC12400-Q1 when I adjust the SCLK polarity to match yours. To verify all your polarity settings are correct, I would suggest using your scope to view and compare the CS, SCLK, and MOSI waveforms from the MSP430 MCU using the GUI with the exact same register read/write from your external MCU.
So to summarize, invert your SCLK polarity and match the SPI waveforms from the GUI and MSP430. And check for sources that may be loading the SPI signals and reducing their amplitude.
Regards,
Jonathan