Part Number: SN75DPHY440SS
Hi
My customer asks us to help review the schematic and layout, I send the file via mail.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DPHY440SS
Hi
My customer asks us to help review the schematic and layout, I send the file via mail.
Hi,
For schematic, please make sure VDD and VREG_OUT are only connected to 100nF pulldown capacitor. You do not need to connect them to external 1.2V.
On the layout, do they want to move the DPHY440 closer to the RX instead putting it in the middle? The DPHY440 as aa re-timer can provide skew compensation at its input. With the current design, it will not able to provide skew compensation for the ~3.5in trace at its output.
Thanks
David