Part Number: DS92LV18
I'm searching for some clarification regarding DS92LV18.
In this application TCLK and REFCLK = 20MHz, generated from an FPGA clock of about 100 MHz.
The expected Duty-Cycle will be 60% or 40% with a pretty strong accuracy (generated from a counter 3 period H and 2 L or vice versa).
These values of Duty-Cycle are the limits reported on the datasheet, they tested the device on the EVM without any problem, but wanted a further confirmation if in the real board could appear some lock issues or malfunctions.
Please let me know if from your side some problem can appear.
Thanks in advance
Matteo