Part Number: SN65MLVD204A
10.2.2.7 Receiver Input Threshold (Failsafe) Measured to confirm that it is as specified.
A FET probe was used to measure the differential output.
If the -A and -B terminals are shorted together, will this kind of failure mode occur?
-Will this kind of failure mode occur if the A terminal and GND terminal are shorted?
-Will this failure mode occur if the B terminal and VDD terminal are shorted?