This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
Normal CAN is usually recorded at 500HZ, when using CAN FD customer always use 1MHZ, is there an application document that describes the design of peripheral circuits for CAN and CANFD? Does this require modifying the parameters of the peripheral circuit? such as the values of capacitance or resistance, thanks.
Hi Hangjie,
You can use TCAN1043A EVM as a reference. For 500Hz and 1Mhz there won't be difference.
Attached is a draft, which will be used as internal reference in the future. I'm still working on it.
Regards,
Sean