Part Number: TFP410
Tool/software:
Hi,
Is the TFP410 deterministic internally - if I have two devices clocked by the same source with the same contol signals (DE/xSYNC) and I provide input data that is well-timed and synchronous, would it be reasonable to use two devices to provide a dual-link DVI connection? (CK output from the second device being unused)
Asked another way, if I fed two TFP410 devices with identical inputs would their outputs be guaranteed to be identical ie there is no metastability resolution/clock domain crossing within the part?
What if reset is asynchronous to each part? What if the two parts are accessed over I2C at different times? Do the outputs depend only on the current inputs with a fixed number of pipeline delays?
Many thanks,
Paul