Part Number: TMUXHS4212
Tool/software:
Hi Sir,
We have a project that refers to an old version of the datasheet, so RESVD* is not connected to VCC, so it will enter test mode when used..
Now that we cannot modify the hardware design, could you provide the relevant control flow to eliminate entering test mode?
Case 1:
Is it possible to toggle the OEn pin before entering test mode to destroy the number of toggles of the SEL pin?
Like, Power on => OEn set to "L" => SEL toggle 10 times => OEn set to "H" then to "L" => SEL toggle 10 times => OEn set to "H" then to "L" => .....
Is it possible to use this method to avoid entering test mode? Do we need to add waiting time to each stage?
Case 2:
How to return to normal mode if TMUXHS4212 is already in test mode? Could you please confirm whether the following control process is correct?
In the test mode => power off => power on => OEn set to "L" => back to normal mode?
Do we need to add waiting time to each stage?
Thank you~~
Baw