Part Number: SN65HVD70
Tool/software:
Hello Team,
We are using SN65HVD70D in our application. Can you provide the characteristic impedance for RS422 differential signal lines?
Thank You.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This device is designed for loads between 54 Ω and 100 Ω. This allows for signal lines with a characteristic differential impedance of 100 Ω (typically used for unidirectional RS-422 with one termination resistor) or 120 Ω (typically used for half-duplex RS-485 with two termination resistors).
I see I am a little late to this post, but Clemens is spot on here. Because this device is compliant with both RS-485 (54Ohms) and RS-422 (100Ohms) standards, it can support both characteristic impedances. Just make sure to add termination resistors correctly. This article can help: www.ti.com/.../SSZTB23
-Ethan