Part Number: DS125MB203
Tool/software:
Hello:
At present, it takes a long time for us to switch between GPON and EPON. We hope to achieve the effect of 1in->2out through the BUFFER DS125MB203. The signal coming in from SFP may be GPON signal or EPON signal. The signal coming in from SFP+ may be XGPON or 10GEPON signal. We originally only received 2 SerDes, but now we hope to receive 4 at the same time through DS125MB203. In this way, whether it is GPON + XGPON or EPON + 10GEPON, I can receive them at the same time.
Attached is the block diagram I drew and the questions I asked. There is also the schematic diagram of my test adapter board. Can you help me check if there is any problem with the principle? It is mainly the capacitive coupling of the front and rear stages, combined with the recommended design in my block diagram.
In addition, is my application feasible and is there any recommended configuration?