Part Number: TSB41BA3F-EP
Tool/software:
Hello,
I am working on a new design to use the TSB41BA3F PHY. During testing, I am able to communicate with the internal PHY registers and configure all of the ports.
However, when I connect the PHY to any other 1394 device (the results are the same for S100,S200, & S400 as well beta and alpha only devices, for all ports for all power classes), the PHY seems to cause continual bus resets, and 'kills' the rest of the bus.
This occurs when bRESET is held high, so that the PHY is not in reset, but the LPS and other pins are held low (so that only the PHY is active, not my custom Link)
I would appreciate any recommendations as to why the PHY is not able to complete the bus initialization / sequence even when there is no attached link.