Other Parts Discussed in Thread: LSF0102, TCA39306, TCA9617B
Tool/software:
Hi TI team,
Originally, I would like to use TCA9509 as voltage translator of 5V<-->3.3V, but when I checked the details, I found VIL of TCA9509 is 110mV, which is too low for slave 6# in below schematic.
Can you kindly recommend an option with higher VIL? For example, 0.8V or higher.
By the way, what's the VIL&VOL of LSF0102 ? Is it OK to use LSF0102 instead?
Thank you.

Kind Regards,
Bo