Tool/software:
The DS90UB941 configuration register combined with the DS90UB948 outputs 1920*1080 images,
But refer to the programming example of zhcaag5a.pdf manual to modify, the specific register is written as follows, but it can not be displayed on the screen, and read 0x06 register through 941 address can not read the address of the unstring 948, directly read with 948 address, The returned status value is STATUS_I2C_RECEIVED_NACK, there is no idea, please guide to deal with it, thank you
Hello!
I will be referencing the 941AS bring up guide for some further analysis of this setup: DS90UB941AS-Q1 DSI Bringup Guide
From the script that is provided, I am seeing the following configurations:
serAddr = 0x18 # Disable the DSI input board.WriteI2c(serAddr, 0x01, 0x08) board.WriteI2c(serAddr, 0x1E, 0x01) # TX port select, Port 0 selected # Continuous DSI CLK # Dual DSI # DSI Port 0 # Alternate Lines 3D Mode # 4 Lanes board.WriteI2C(serAddr, 0x4F, 0xDC) # Dual Config Registers - FPDTX mode = Forced splitter mode board.WriteI2C(serAddr, 0x5B, 0x07) # Left/Right 3D Processing board.WriteI2C(serAddr, 0x56, 0x80) board.WriteI2C(serAddr, 0x32, 0x80) # IMG_LINE_SIZE0 processing board.WriteI2C(serAddr, 0x33, 0x07) # IMG_LINE_SIZE1 processing # IMG Line processing set to 1920 px board.WriteI2c(serAddr, 0x1E, 0x01) # TX port select, Port 0 selected (again) board.WriteI2C(serAddr, 0x1E, 0x01) # TX port select, Port 0 selected (again) board.WriteI2C(serAddr, 0x36, 0x00) # Crop Start X axis (0) - LSB = 0 board.WriteI2C(serAddr, 0x37, 0x80) # Crop Start X axis (1) - Crop enable, MSB = 0 board.WriteI2C(serAddr, 0x38, 0x7F) # Crop Stop X axis (0) - LSB = 0111 0111 board.WriteI2C(serAddr, 0x39, 0x07) # Crop Stop X axis (1) - MSB = 0111 # Crop start at 0 goes to 1919 board.WriteI2C(serAddr, 0x3A, 0x00) # Crop Start Y axis (0) - LSB = 0 board.WriteI2C(serAddr, 0x3B, 0x00) # Crop Start Y axis (1) - MSB = 0 board.WriteI2C(serAddr, 0x3C, 0x37) # Crop Stop Y axis (0) - LSB = 0011 0111 board.WriteI2C(serAddr, 0x3D, 0x04) # Crop Stop Y axis (1) - MSB = 0100 # Crop start at 0 goes to 1079 board.WriteI2C(serAddr, 0x40, 0x04) # DSI/DPHY Port 0 Registers board.WriteI2C(serAddr, 0x41, 0x05) # DPHY Skip timing board.WriteI2C(serAddr, 0x42, 0x1E) # Set to dec = 15 # Enable DSI board.WriteI2C(serAddr, 0x01, 0x00)
Can you please confirm the DSI configuration being used, the FPD Link topology, and the DSI rate for the appropriate configurations?
One suggestion I have is to ensure that the correct polarity is selected for the DES / display configuration, this can be done through the following registers on the DSI indirect page registers:
board.WriteI2C(serAddr,0x40,0x04) # Set HSYNC/VSYNC Polarity DSI0 board.WriteI2C(serAddr,0x41,0x21) # Set HSYNC/VSYNC Polarity DSI0 board.WriteI2C(serAddr,0x42,0x60) # Set HSYNC/VSYNC Polarity DSI0
Additionally, please ensure that the DSI clock settings are configured properly from section 10.2 of the datasheet:
board.WriteI2C(serAddr,0x40,0x10) # Init DSI Clock Settings (From Section 10.2 of datasheet) board.WriteI2C(serAddr,0x41,0x86) # Init DSI Clock Settings (From Section 10.2 of datasheet) board.WriteI2C(serAddr,0x42,0x0A) # Init DSI Clock Settings (From Section 10.2 of datasheet) board.WriteI2C(serAddr,0x41,0x94) # Init DSI Clock Settings (From Section 10.2 of datasheet) board.WriteI2C(serAddr,0x42,0x0A) # Init DSI Clock Settings (From Section 10.2 of datasheet)
It is also a good idea to digital reset the 948 after initialization in order to restart the AEQ (put this at the end):
desAddr = 0x58 board.WriteI2C(UB948,0x01,0x01) # Digital reset to restart AEQ
and read 0x06 register through 941 address can not read the address of the unstring 948, directly read with 948 address, The returned status value is STATUS_I2C_RECEIVED_NACK
If you cannot read the device ID, it may be that RX Lock is not established. Can you check on the 948 side to ensure the device can be remotely accessed? I am thinking the connection from 941 to 948 may not be established due to hardware configuration. Please check LOCK/PASS status on the 948 to confirm the connection (Pin 1 and Pin 7).
Let me know if any clarifications are needed here!
Best,
Miguel
1. 941 and 948 can be locked after power-on, but TI941_WriteRegister(IDX_941, 0x01, 0x08) when starting to configure the 941 register; And TI941_WriteRegister(IDX_941, 0x4F, 0xDC); So the register will cause the Lock to disconnect, and can not restore the normal connection state, why?
2. According to your above Pointers, reconfigure the register 0x41,0x42, then how to configure the corresponding relevant data, because I did not find the reference article, I finally need to output is 1920*1080 screen
Hello!
941 and 948 can be locked after power-on, but TI941_WriteRegister(IDX_941, 0x01, 0x08) when starting to configure the 941 register; And TI941_WriteRegister(IDX_941, 0x4F, 0xDC); So the register will cause the Lock to disconnect, and can not restore the normal connection state, why?
Yes, this is expected behavior, the first write (0x01=0x08) disables the DSI input, the second write sets the DSI configuration. While the DSI is disabled, there is no input to the RX of the 941 SER, meaning no valid video throughput to the 948.
At this time, the 948 will sample whether valid video is incoming to certify whether lock is established based on register 0x34 bit 6: RX_LOCK_MODE
This explains why the lock status is not established as DSI is being configured.
According to your above Pointers, reconfigure the register 0x41,0x42, then how to configure the corresponding relevant data, because I did not find the reference article, I finally need to output is 1920*1080 screen
I recommend referring to the DS90UB941AS-Q1 DSI Bringup Guide for specific configuration assistance, as I see splitter mode is being implemented here with cropping to two displays.
In the debug section, it is recommended to first test the internal pattern generation in order to certify the connection from SER -> DES -> Display is working appropriately, in a topology of SER -> DES -> x1 Display at 1920x1080p, a pattern script can be generated with the register assignments in Exploring the Int Test Pattern Generation Feature of FPD-Link III IVI Devices (Rev. G).
If you need, I can help generate this script, but I believe the pattern generated will only go to one display (in which I will need the display specification for all timing parameters).
Please let me know what assistance you may need from here!
Best,
Miguel
How should I configure which registers? 1920*1080 is the image output, and the clock frequency is 142MHz-158MHz. Can you help me configure the specific registers
Hello!
I can help you evaluate this configuration; can you please provide an example of flower screen or describe the exact abnormality for documentation purposes?
Per the debugging flow of the bring up guide (https://www.ti.com/lit/an/snla356/snla356.pdf?ts=1740076915839), I am providing a PATGEN script, which will be internally generated through the 941AS send directly to the 948. Can you please double confirm the topology used by providing a block diagram?
1920*1080 is the image output, and the clock frequency is 142MHz-158MHz
I may also need the display timing specifications to prevent any issues from the video timing on the display side, but I have provided a default 1920 x 1080 resolution at 60 fps (148.5 MHz PCLK) PATGEN.
Please refer to the script below for these register writes:
devAddr = 0x18 PGIA = 0x66 PGID = 0x67 board.WriteI2C(0x01, 0x08) # Disable DSI input board.WriteI2C(0x1E, 0x01) # TX Port Select = FPD Port 0 Sel board.WriteI2C(0x5B, 0x03) # TX Mode = Forced Dual FPD-Link III Transmitter mode # Populate based on expected display timings PGRS = 0x00 PGGS = 0x00 PGBS = 0x00 PGCDC1 = 0x02 PGCDC2 = 0x98 PGTFS1 = 0x58 PGTFS2 = 0x46 PGTFS3 = 0x80 PGAFS1 = 0x87 PGAFS2 = 0x43 PGAFS3 = 0x2C PGHSW = 0x05 PGVSW = 0x94 PGHBP = 0x24 PGVBP = 0x00 PBSC = 0x1E PGFT = 0x0C PFTSC = 0x21 PGTS01 = 0x43 PGTS02 = 0x65 PGTS03 = 0x87 PGTS04 = 0xA9 PGTS05 = 0xCB PGTS06 = 0xED PGTS07 = 0x0F PGTS08 = 0x00 PGBE = 0x01 PGCDC2 = 0x00 board.WriteI2C(devAddr, PGIA, 0x00) board.WriteI2C(devAddr, PGID, PGRS) #PGRS board.WriteI2C(devAddr, PGIA, 0x01) board.WriteI2C(devAddr, PGID, PGGS) #PGGS board.WriteI2C(devAddr, PGIA, 0x02) board.WriteI2C(devAddr, PGID, PGBS) #PGBS board.WriteI2C(devAddr, PGIA, 0x03) board.WriteI2C(devAddr, PGID, PGCDC1) #PGCDC1 board.WriteI2C(devAddr, PGIA, 0x04) board.WriteI2C(devAddr, PGID, PGTFS1) #PGTFS1 board.WriteI2C(devAddr, PGIA, 0x05) board.WriteI2C(devAddr, PGID, PGTFS2) #PGTFS2 board.WriteI2C(devAddr, PGIA, 0x06) board.WriteI2C(devAddr, PGID, PGTFS3) #PGTFS3 board.WriteI2C(devAddr, PGIA, 0x07) board.WriteI2C(devAddr, PGID, PGAFS1) #PGAFS1 board.WriteI2C(devAddr, PGIA, 0x08) board.WriteI2C(devAddr, PGID, PGAFS2) #PGAFS2 board.WriteI2C(devAddr, PGIA, 0x09) board.WriteI2C(devAddr, PGID, PGAFS3) #PGAFS3 board.WriteI2C(devAddr, PGIA, 0x0a) board.WriteI2C(devAddr, PGID, PGHSW) #PGHSW board.WriteI2C(devAddr, PGIA, 0x0b) board.WriteI2C(devAddr, PGID, PGVSW) #PGVSW board.WriteI2C(devAddr, PGIA, 0x0c) board.WriteI2C(devAddr, PGID, PGHBP) #PGHBP board.WriteI2C(devAddr, PGIA, 0x0d) board.WriteI2C(devAddr, PGID, PGVBP) #PGVBP board.WriteI2C(devAddr, PGIA, 0x0e) board.WriteI2C(devAddr, PGID, PBSC) #PBSC, if not working try both positive AND negative polarity board.WriteI2C(devAddr, PGIA, 0x0f) board.WriteI2C(devAddr, PGID, PGFT) #PGFT board.WriteI2C(devAddr, PGIA, 0x10) board.WriteI2C(devAddr, PGID, PGTSC) #PGTSC board.WriteI2C(devAddr, PGIA, 0x11) board.WriteI2C(devAddr, PGID, PGTS01) #PGTS01 board.WriteI2C(devAddr, PGIA, 0x12) board.WriteI2C(devAddr, PGID, PGTS02) #PGTS02 board.WriteI2C(devAddr, PGIA, 0x13) board.WriteI2C(devAddr, PGID, PGTS03) #PGTS03 board.WriteI2C(devAddr, PGIA, 0x14) board.WriteI2C(devAddr, PGID, PGTS04) #PGTS04 board.WriteI2C(devAddr, PGIA, 0x15) board.WriteI2C(devAddr, PGID, PGTS05) #PGTS05 board.WriteI2C(devAddr, PGIA, 0x16) board.WriteI2C(devAddr, PGID, PGTS06) #PGTS06 board.WriteI2C(devAddr, PGIA, 0x17) board.WriteI2C(devAddr, PGID, PGTS07) #PGTS07 board.WriteI2C(devAddr, PGIA, 0x18) board.WriteI2C(devAddr, PGID, PGTS08) #PGTS08 board.WriteI2C(devAddr, PGIA, 0x19) board.WriteI2C(devAddr, PGID, PGBE) #PGBE board.WriteI2C(devAddr, PGIA, 0x1a) board.WriteI2C(devAddr, PGID, PGCDC2) #PGCDC2 board.WriteI2C(devAddr, 0x65, 0x00) board.WriteI2C(devAddr, 0x64, 0x05)
In this case, you may replace devAddr with IDX_941 as used in your script.
For further clarification on these configuration registers, please see Exploring the Int Test Pattern Generation Feature of FPD-Link III IVI Devices (Rev. G)
Since PATGEN will be internally generated at the 941, there is no need for DSI configuration at this time - we are testing the link between SER -> DES -> Display independent of the source.
Please let me know the results of the testing, then we can proceed to next steps to resolve display abnormalities.
Thanks,
Miguel
1、Our project is to input MIPI to LVDS output 1920*1080. Through the example of output internal color bar chart provided by you, the color bar chart can be output normally after testing.1920*1080 is the image output, and the clock frequency is 142MHz-158MHz;
2、The above is my configuration of the 941 register, through the above configuration, the output screen appears flower screen;
3、In order to be able to output 1920*1080 video normally, how should I configure, please guide me, more eager,thank you!
Hello,
Thank you for testing this - it appears that the internal PATGEN from the 941AS confirms that the FPD-Link between 941AS and 948 is configured correctly. I will now focus on the DSI RX register configuration.
Can you please confirm or provide the following information? I will review the code you have provided above in the meantime.
Looking forward to your reply!
Best,
Miguel
1、Continuous DSI CLK
2、Single DSI input, dual output
3、Not alternate line 3D mode
4、4 Number of DSI channels
5、DSI rate (Mbps): 290Mbps
Thank you for this information, I will provide feedback for the code above momentarily.
Best,
Miguel
Hello,
Thanks for this information, we will need this for a later step in the debug.
Through the example of output internal color bar chart provided by you, the color bar chart can be output normally after testing.1920*1080 is the image output, and the clock frequency is 142MHz-158MHz
For the time being we can now proceed with the flow diagram now that PATGEN from SER is successful (from DS90UB941AS-Q1 DSI Bringup Guide):
The next script will confirm if the clock is correct and using internal timing (data lanes are not applied).
devAddr = 0x18 PGIA = 0x66 PGID = 0x67 board.WriteI2C(0x01, 0x08) # Disable DSI input board.WriteI2C(0x1E, 0x01) # TX Port Select = FPD Port 0 Sel board.WriteI2C(0x5B, 0x03) # TX Mode = Forced Dual FPD-Link III Transmitter mode # Populate based on expected display timings PGRS = 0x00 PGGS = 0x00 PGBS = 0x00 PGCDC1 = 0x02 PGCDC2 = 0x98 PGTFS1 = 0x58 PGTFS2 = 0x46 PGTFS3 = 0x80 PGAFS1 = 0x87 PGAFS2 = 0x43 PGAFS3 = 0x2C PGHSW = 0x05 PGVSW = 0x94 PGHBP = 0x24 PGVBP = 0x00 PBSC = 0x1E PGFT = 0x0C PFTSC = 0x21 PGTS01 = 0x43 PGTS02 = 0x65 PGTS03 = 0x87 PGTS04 = 0xA9 PGTS05 = 0xCB PGTS06 = 0xED PGTS07 = 0x0F PGTS08 = 0x00 PGBE = 0x01 PGCDC2 = 0x00 board.WriteI2C(devAddr, PGIA, 0x00) board.WriteI2C(devAddr, PGID, PGRS) #PGRS board.WriteI2C(devAddr, PGIA, 0x01) board.WriteI2C(devAddr, PGID, PGGS) #PGGS board.WriteI2C(devAddr, PGIA, 0x02) board.WriteI2C(devAddr, PGID, PGBS) #PGBS board.WriteI2C(devAddr, PGIA, 0x03) board.WriteI2C(devAddr, PGID, PGCDC1) #PGCDC1 board.WriteI2C(devAddr, PGIA, 0x04) board.WriteI2C(devAddr, PGID, PGTFS1) #PGTFS1 board.WriteI2C(devAddr, PGIA, 0x05) board.WriteI2C(devAddr, PGID, PGTFS2) #PGTFS2 board.WriteI2C(devAddr, PGIA, 0x06) board.WriteI2C(devAddr, PGID, PGTFS3) #PGTFS3 board.WriteI2C(devAddr, PGIA, 0x07) board.WriteI2C(devAddr, PGID, PGAFS1) #PGAFS1 board.WriteI2C(devAddr, PGIA, 0x08) board.WriteI2C(devAddr, PGID, PGAFS2) #PGAFS2 board.WriteI2C(devAddr, PGIA, 0x09) board.WriteI2C(devAddr, PGID, PGAFS3) #PGAFS3 board.WriteI2C(devAddr, PGIA, 0x0a) board.WriteI2C(devAddr, PGID, PGHSW) #PGHSW board.WriteI2C(devAddr, PGIA, 0x0b) board.WriteI2C(devAddr, PGID, PGVSW) #PGVSW board.WriteI2C(devAddr, PGIA, 0x0c) board.WriteI2C(devAddr, PGID, PGHBP) #PGHBP board.WriteI2C(devAddr, PGIA, 0x0d) board.WriteI2C(devAddr, PGID, PGVBP) #PGVBP board.WriteI2C(devAddr, PGIA, 0x0e) board.WriteI2C(devAddr, PGID, PBSC) #PBSC, if not working try both positive AND negative polarity board.WriteI2C(devAddr, PGIA, 0x0f) board.WriteI2C(devAddr, PGID, PGFT) #PGFT board.WriteI2C(devAddr, PGIA, 0x10) board.WriteI2C(devAddr, PGID, PGTSC) #PGTSC board.WriteI2C(devAddr, PGIA, 0x11) board.WriteI2C(devAddr, PGID, PGTS01) #PGTS01 board.WriteI2C(devAddr, PGIA, 0x12) board.WriteI2C(devAddr, PGID, PGTS02) #PGTS02 board.WriteI2C(devAddr, PGIA, 0x13) board.WriteI2C(devAddr, PGID, PGTS03) #PGTS03 board.WriteI2C(devAddr, PGIA, 0x14) board.WriteI2C(devAddr, PGID, PGTS04) #PGTS04 board.WriteI2C(devAddr, PGIA, 0x15) board.WriteI2C(devAddr, PGID, PGTS05) #PGTS05 board.WriteI2C(devAddr, PGIA, 0x16) board.WriteI2C(devAddr, PGID, PGTS06) #PGTS06 board.WriteI2C(devAddr, PGIA, 0x17) board.WriteI2C(devAddr, PGID, PGTS07) #PGTS07 board.WriteI2C(devAddr, PGIA, 0x18) board.WriteI2C(devAddr, PGID, PGTS08) #PGTS08 board.WriteI2C(devAddr, PGIA, 0x19) board.WriteI2C(devAddr, PGID, PGBE) #PGBE board.WriteI2C(devAddr, PGIA, 0x1a) board.WriteI2C(devAddr, PGID, PGCDC2) #PGCDC2 board.WriteI2C(devAddr, 0x65, 0x0C) board.WriteI2C(devAddr, 0x64, 0x05)
While the DSI source is enabled, it will only be providing clock in this scenario, as options of External Clock Source is enabled and Timing is generated and configured internally.
Please let me know the results of this test, and we may proceed with understanding where the phenomenon is occurring from.
Best,
Miguel
After writing according to the script you provided, there was no image output on the display screen, and PGTSC did not have the corresponding value in the script you provided. I set PGTSC=0 for the test. The detailed code is as follows:
TI941_WriteRegister(IDX_941, 0x01, 0x08); /* Disable DSI input */
TI941_WriteRegister(IDX_941, 0x1E, 0x01); /* TX Port Select = FPD Port 0 Sel */
TI941_WriteRegister(IDX_941, 0x5B, 0x03); /* TX Mode = Forced Dual FPD-Link III Transmitter mode */
TI941_WriteRegister(IDX_941, 0x66, 0x00);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x66, 0x01);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x66, 0x02);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x66, 0x03);
TI941_WriteRegister(IDX_941, 0x67, 0x02);
TI941_WriteRegister(IDX_941, 0x66, 0x04);
TI941_WriteRegister(IDX_941, 0x67, 0x58);
TI941_WriteRegister(IDX_941, 0x66, 0x05);
TI941_WriteRegister(IDX_941, 0x67, 0x46);
TI941_WriteRegister(IDX_941, 0x66, 0x06);
TI941_WriteRegister(IDX_941, 0x67, 0x80);
TI941_WriteRegister(IDX_941, 0x66, 0x07);
TI941_WriteRegister(IDX_941, 0x67, 0x87);
TI941_WriteRegister(IDX_941, 0x66, 0x08);
TI941_WriteRegister(IDX_941, 0x67, 0x43);
TI941_WriteRegister(IDX_941, 0x66, 0x09);
TI941_WriteRegister(IDX_941, 0x67, 0x2C);
TI941_WriteRegister(IDX_941, 0x66, 0x0a);
TI941_WriteRegister(IDX_941, 0x67, 0x05);
TI941_WriteRegister(IDX_941, 0x66, 0x0b);
TI941_WriteRegister(IDX_941, 0x67, 0x94);
TI941_WriteRegister(IDX_941, 0x66, 0x0C);
TI941_WriteRegister(IDX_941, 0x67, 0x24);
TI941_WriteRegister(IDX_941, 0x66, 0x0D);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x66, 0x0E);
TI941_WriteRegister(IDX_941, 0x67, 0x1E);
TI941_WriteRegister(IDX_941, 0x66, 0x0F);
TI941_WriteRegister(IDX_941, 0x67, 0x0C);
TI941_WriteRegister(IDX_941, 0x66, 0x10);
TI941_WriteRegister(IDX_941, 0x67, 0x00); // PGTSC
TI941_WriteRegister(IDX_941, 0x66, 0x11);
TI941_WriteRegister(IDX_941, 0x67, 0x43);
TI941_WriteRegister(IDX_941, 0x66, 0x12);
TI941_WriteRegister(IDX_941, 0x67, 0x65);
TI941_WriteRegister(IDX_941, 0x66, 0x13);
TI941_WriteRegister(IDX_941, 0x67, 0x87);
TI941_WriteRegister(IDX_941, 0x66, 0x14);
TI941_WriteRegister(IDX_941, 0x67, 0xA9);
TI941_WriteRegister(IDX_941, 0x66, 0x15);
TI941_WriteRegister(IDX_941, 0x67, 0xCB);
TI941_WriteRegister(IDX_941, 0x66, 0x16);
TI941_WriteRegister(IDX_941, 0x67, 0xED);
TI941_WriteRegister(IDX_941, 0x66, 0x17);
TI941_WriteRegister(IDX_941, 0x67, 0x0F);
TI941_WriteRegister(IDX_941, 0x66, 0x18);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x66, 0x19);
TI941_WriteRegister(IDX_941, 0x67, 0x01);
TI941_WriteRegister(IDX_941, 0x66, 0x1A);
TI941_WriteRegister(IDX_941, 0x67, 0x00);
TI941_WriteRegister(IDX_941, 0x65, 0x0C);
TI941_WriteRegister(IDX_941, 0x64, 0x05);
TI941_WriteRegister(IDX_941, 0x01, 0x00); /*Enable DSI*/
Hi,
Let us try using this same script by not disabling the clock -> this TX of the DSI is needed to configure the PATGEN:
TI941_WriteRegister(IDX_941, 0x66, 0x00); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x01); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x02); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x03); TI941_WriteRegister(IDX_941, 0x67, 0x02); TI941_WriteRegister(IDX_941, 0x66, 0x04); TI941_WriteRegister(IDX_941, 0x67, 0x58); TI941_WriteRegister(IDX_941, 0x66, 0x05); TI941_WriteRegister(IDX_941, 0x67, 0x46); TI941_WriteRegister(IDX_941, 0x66, 0x06); TI941_WriteRegister(IDX_941, 0x67, 0x80); TI941_WriteRegister(IDX_941, 0x66, 0x07); TI941_WriteRegister(IDX_941, 0x67, 0x87); TI941_WriteRegister(IDX_941, 0x66, 0x08); TI941_WriteRegister(IDX_941, 0x67, 0x43); TI941_WriteRegister(IDX_941, 0x66, 0x09); TI941_WriteRegister(IDX_941, 0x67, 0x2C); TI941_WriteRegister(IDX_941, 0x66, 0x0a); TI941_WriteRegister(IDX_941, 0x67, 0x05); TI941_WriteRegister(IDX_941, 0x66, 0x0b); TI941_WriteRegister(IDX_941, 0x67, 0x94); TI941_WriteRegister(IDX_941, 0x66, 0x0C); TI941_WriteRegister(IDX_941, 0x67, 0x24); TI941_WriteRegister(IDX_941, 0x66, 0x0D); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x0E); TI941_WriteRegister(IDX_941, 0x67, 0x1E); TI941_WriteRegister(IDX_941, 0x66, 0x0F); TI941_WriteRegister(IDX_941, 0x67, 0x0C); TI941_WriteRegister(IDX_941, 0x66, 0x10); TI941_WriteRegister(IDX_941, 0x67, 0x21); // PGTSC TI941_WriteRegister(IDX_941, 0x66, 0x11); TI941_WriteRegister(IDX_941, 0x67, 0x43); TI941_WriteRegister(IDX_941, 0x66, 0x12); TI941_WriteRegister(IDX_941, 0x67, 0x65); TI941_WriteRegister(IDX_941, 0x66, 0x13); TI941_WriteRegister(IDX_941, 0x67, 0x87); TI941_WriteRegister(IDX_941, 0x66, 0x14); TI941_WriteRegister(IDX_941, 0x67, 0xA9); TI941_WriteRegister(IDX_941, 0x66, 0x15); TI941_WriteRegister(IDX_941, 0x67, 0xCB); TI941_WriteRegister(IDX_941, 0x66, 0x16); TI941_WriteRegister(IDX_941, 0x67, 0xED); TI941_WriteRegister(IDX_941, 0x66, 0x17); TI941_WriteRegister(IDX_941, 0x67, 0x0F); TI941_WriteRegister(IDX_941, 0x66, 0x18); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x19); TI941_WriteRegister(IDX_941, 0x67, 0x01); TI941_WriteRegister(IDX_941, 0x66, 0x1A); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x65, 0x0C); TI941_WriteRegister(IDX_941, 0x64, 0x05);
The PGTSC was not carried over from the previous write as 0x21 - this is corrected (but has no effect, as auto scrolling is disabled).
Since the DSI configuration is not disturbed in this setup, please try this sequence:
This comes from 941 power up sequencing, the suggestion here is to apply the DSI input before initializing with the code above to see if the output will appear. In this way, we can rule out whether the DSI clock is part of the issue in this configuration.
If that does not work, we will need to evaluate the DSI input further based on this portion of the debug flow diagram (DS90UB941AS-Q1 DSI Bringup Guide):
In the case the new code and sequencing is unsuccessful, we may try to evaluate the DSI configurations and continuous clock by checking this section:
I have linked this guide above as well, please let me know if you need any further details testing this.
If the code and sequence works, we can try the next step which is to use the same code but with external timing input:
TI941_WriteRegister(IDX_941, 0x66, 0x00); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x01); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x02); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x03); TI941_WriteRegister(IDX_941, 0x67, 0x02); TI941_WriteRegister(IDX_941, 0x66, 0x04); TI941_WriteRegister(IDX_941, 0x67, 0x58); TI941_WriteRegister(IDX_941, 0x66, 0x05); TI941_WriteRegister(IDX_941, 0x67, 0x46); TI941_WriteRegister(IDX_941, 0x66, 0x06); TI941_WriteRegister(IDX_941, 0x67, 0x80); TI941_WriteRegister(IDX_941, 0x66, 0x07); TI941_WriteRegister(IDX_941, 0x67, 0x87); TI941_WriteRegister(IDX_941, 0x66, 0x08); TI941_WriteRegister(IDX_941, 0x67, 0x43); TI941_WriteRegister(IDX_941, 0x66, 0x09); TI941_WriteRegister(IDX_941, 0x67, 0x2C); TI941_WriteRegister(IDX_941, 0x66, 0x0a); TI941_WriteRegister(IDX_941, 0x67, 0x05); TI941_WriteRegister(IDX_941, 0x66, 0x0b); TI941_WriteRegister(IDX_941, 0x67, 0x94); TI941_WriteRegister(IDX_941, 0x66, 0x0C); TI941_WriteRegister(IDX_941, 0x67, 0x24); TI941_WriteRegister(IDX_941, 0x66, 0x0D); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x0E); TI941_WriteRegister(IDX_941, 0x67, 0x1E); TI941_WriteRegister(IDX_941, 0x66, 0x0F); TI941_WriteRegister(IDX_941, 0x67, 0x0C); TI941_WriteRegister(IDX_941, 0x66, 0x10); TI941_WriteRegister(IDX_941, 0x67, 0x21); // PGTSC TI941_WriteRegister(IDX_941, 0x66, 0x11); TI941_WriteRegister(IDX_941, 0x67, 0x43); TI941_WriteRegister(IDX_941, 0x66, 0x12); TI941_WriteRegister(IDX_941, 0x67, 0x65); TI941_WriteRegister(IDX_941, 0x66, 0x13); TI941_WriteRegister(IDX_941, 0x67, 0x87); TI941_WriteRegister(IDX_941, 0x66, 0x14); TI941_WriteRegister(IDX_941, 0x67, 0xA9); TI941_WriteRegister(IDX_941, 0x66, 0x15); TI941_WriteRegister(IDX_941, 0x67, 0xCB); TI941_WriteRegister(IDX_941, 0x66, 0x16); TI941_WriteRegister(IDX_941, 0x67, 0xED); TI941_WriteRegister(IDX_941, 0x66, 0x17); TI941_WriteRegister(IDX_941, 0x67, 0x0F); TI941_WriteRegister(IDX_941, 0x66, 0x18); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x66, 0x19); TI941_WriteRegister(IDX_941, 0x67, 0x01); TI941_WriteRegister(IDX_941, 0x66, 0x1A); TI941_WriteRegister(IDX_941, 0x67, 0x00); TI941_WriteRegister(IDX_941, 0x65, 0x08); TI941_WriteRegister(IDX_941, 0x64, 0x05);
This code will then determine if all SoC configurations are coming into the 941 correctly.
If you have any further questions or concerns, please let me know.
Best,
Miguel
Hi,
When receiving the STATUS_I2C_RECEIVED_NACK, this indicates that there may be an issue with the link between the SER and DES device.
Is the 948 devices always remotely accessed from the 941 SER? If these transactions are failing, this could indicate an issue on the LOCK stability and status between the SER / DES devices.
Best,
Miguel
I configured the register of 941 to output the screen of 1920*1080 through the 948 unstring chip. At present, the screen always appears and the register read through the address of the 948 unstring reader always returns STATUS_I2C_RECEIVED_NACK, but the color bar chart can be displayed through the configuration of 941
1、I configured the register of 941 to output the screen of 1920*1080 through the 948 unstring chip. At present, the screen always appears and the register read through the address of the 948 unstring reader always returns STATUS_I2C_RECEIVED_NACK, but the color bar chart can be displayed through the configuration of 941.
2、948 is set to 0V and R2 is set to 10kΩ. According to the specifications, IDx should be 0x2C. However, I directly connected the MCU to the i2c interface of 948 to read the register of 0xF3 using the address 0x2C, and the return value was STATUS_I2C_RECEIVED_NACK. Using IDx as 0x0C to read the register of 0xF3 does return a successfully readable value, what is the reason? Normal 948 address should be 0x2C, checked the hardware can not find the reason
3、This is the 941 schematic:
4、This is the 948 schematic:
Hello,
Allow me to look into this further, it appears that the mode select strap setting for the 941 does not match the following configuration below?
4、4 Number of DSI channels
5、DSI rate (Mbps): 290Mbps
Mode 0 in this case would be 1 lane, but 4 DSI channels are being used here.
MCU to the i2c interface of 948 to read the register of 0xF3 using the address 0x2C, and the return value was STATUS_I2C_RECEIVED_NACK. Using IDx as 0x0C to read the register of 0xF3 does return a successfully readable value
Can you please provide whether the I2C commands from the MCU would read in 7-bit or 8-bit addressing? For example, our ALP tool for the 94x devices will read and communicate in 8-bit IDx addresses:
Please let me know, I will continue to evaluate the configuration settings offline, if you are still unable to access the 948 remotely there may be an issue with the backchannel configurations that may need to be evaluated.
From there, we will continue to look at the DSI CLK source to ensure it is good according to the investigation from reading DSI_VC_DTYPE.
Best,
Miguel
1、We have one DSI0 input, two link output, four data channels
2、Address = 0x4F DSI channel select 1, the screen is not displayed, select 4, the screen is displayed only flower screen
3、I use an NXP S32K144 chip, which uses a 7-bit address
Hi,
I see,
We have one DSI0 input, two link output, four data channels
Four data channels and dual (two) FPD-Link configuration, you may need MODE_SEL0 = Mode No. 3
MODE_SEL1 is also set to Mode 7, meaning the DSI will be disabled upon startup.
Address = 0x4F DSI channel select 1, the screen is not displayed, select 4, the screen is displayed only flower screen
I believe this is progress; the lanes should be selected at 4 in order to get any data - but maybe a configuration is causing the flower screen.
TI941_WriteRegister(IDX_941, 0x42, 0x04); TI941_WriteRegister(IDX_941, 0x41, 0x2A); TI941_ReadRegister(IDX_941, 0x42);
I use an NXP S32K144 chip, which uses a 7-bit address
Using IDx as 0x0C to read the register of 0xF3 does return a successfully readable value, what is the reason?
I agree that this is not one of the available addresses on the 948, and is unusual behavior. I am unsure about the reason that only 0x0C works to read the I2C address, are you certain that the address being read here is not the 7-bit address of the 941AS?
To verify this, you can read register 0x00, it should return the programmed IDx address of that device.
Best,
Miguel
1、Are you able to read indirect page register DSI_VC_DTYPE?
Write 0x40 = 0x04 for DSI Port 0
Write 0x41 = 0x2A
Read 0x42 (DSI_VC_DTYPE)
Reading 0x42 yields a value of 0x3E
2、Are you able to provide waveforms to certify the incoming clock and data to the RX is meeting 941AS specifications?
This is the waveform of the 941 RX,
MIPI-CKN to GND test
3、The comparison diagram displayed on the 1920*1080 display after stringing through 941/948 is as follows. The graph displayed after stringing through is stretched horizontally and vertically with different regular deformations
4、Four data channels and dual (two) FPD-Link configuration, you may need MODE_SEL0 = Mode No. 3
MODE_SEL1 is also set to Mode 7, meaning the DSI will be disabled upon startup.
The hardware is configured according to this information, and the output screen is still a flower screen, which is the same as the previous effect
Hi,
Thank you very much for providing all the additional information about the system.
The DSI frequency reported in the oscilloscope capture appears to be around 505.35 MHz,
DSI rate (Mbps): 290Mbps
fDSI = 492 MHz
One of these must be incorrect? I believe the data rate to frequency conversion is a multiple of two, so for a data rate of 290 Mbps = approximately 580 MHz DSI clock frequency.
fPCLK = (fDSI*NLANES)/12
PCLK = 193.33 MHz
If this is the case, the UB948 has a PCLK limitation of 192 MHz in dual-link configuration on the FPD-Link RX side, so this may not work.
- - - - - - - - - -
For the DSI frequency that is shown in the oscilloscope capture, this would be a calculation of
fPCLK = (fDSI*NLANES)/12
PCLK = 168.45 MHz
This is fine, but for this configuration T_SKIP is a different number
With 505.35 MHz / 252.675 Mbps DSI data rate
TSKIP_CNT = Round(65*fDSI - 5)
= 28
board.WriteI2C(serAddr, 0x40, 0x04) # DSI/DPHY Port 0 Registers board.WriteI2C(serAddr, 0x41, 0x05) # DPHY Skip timing board.WriteI2C(serAddr, 0x42, 0x38) # Set to dec = 28
With 580 MHz / 290 Mbps DSI data rate
TSKIP_CNT = Round(65*fDSI - 5)
= 33
board.WriteI2C(serAddr, 0x40, 0x04) # DSI/DPHY Port 0 Registers board.WriteI2C(serAddr, 0x41, 0x05) # DPHY Skip timing board.WriteI2C(serAddr, 0x42, 0x42) # Set to dec = 33
What is the configuration that allows the screen to produce normal (original drawing)?
Best,
Miguel
1、Using 505.35 MHz and 580 MHz calculated values board.WriteI2C(serAddr, 0x42, 0x38) and board.WriteI2C(serAddr, 0x42, 0x42), the effect is still the same, the screen is still displayede
2、What is the configuration that allows the screen to produce normal (original drawing)?
The question is to compare the effect of the dot plot I made on the computer and the result displayed on the 1920*1080 screen through the serializer output
3、This is the register script for the current setup
Hi
Can you please confirm the correct DSI frequency and rate of the SoC and the display timing specifications?
I am unsure if 505.35 MHz is the correct rate or if 580 MHz is the correct rate.
I believe we will need to match the SER/DES PCLK rate to the DSI rate, and the PCLK of the SER/DES to the display.
Thanks,
Miguel
1、This is DSI frequency and rate of the SoC and the display timing specifications
disp_timings1: display-timings {
dsi1_timing0: timing0 {
clock-frequency = <148500000>;
hactive = <1920>;
vactive = <1080>;
hback-porch = <148>;
hfront-porch = <88>;
hsync-len = <44>;
vback-porch = <4>;
vfront-porch = <36>;
vsync-len = <5>;
pixelclk-active = <0>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <0>;
};
};
// (1 << 0) - MIPI_DSI_MODE_VIDEO /* video mode */
// (1 << 1) - MIPI_DSI_MODE_VIDEO_BURST /* video burst mode */
// (1 << 2) - MIPI_DSI_MODE_VIDEO_SYNC_PULSE /* video pulse mode */
// (1 << 3) - MIPI_DSI_MODE_VIDEO_AUTO_VERT /* enable auto vertical count mode */
// (1 << 4) - MIPI_DSI_MODE_VIDEO_HSE /* enable hsync-end packets in vsync-pulse and v-porch area */
// (1 << 5) - MIPI_DSI_MODE_VIDEO_HFP /* disable hfront-porch area */
// (1 << 6) - MIPI_DSI_MODE_VIDEO_HBP /* disable hback-porch area */
// (1 << 7) - MIPI_DSI_MODE_VIDEO_HSA /* disable hsync-active area */
// (1 << 8) - MIPI_DSI_MODE_VSYNC_FLUSH /* flush display FIFO on vsync pulse */
// (1 << 9) - MIPI_DSI_MODE_EOT_PACKET /* disable EoT packets in HS mode */
// (1 << 10) - MIPI_DSI_CLOCK_NON_CONTINUOUS /* device supports non-continuous clock behavior (DSI spec 5.6.1) */
// (1 << 11) - MIPI_DSI_MODE_LPM /* transmit data in low power */
dsi,flags = <((1 << 0) | (1 << 1) | (1 << 11) | (1 << 9))>;
// 0 - MIPI_DSI_FMT_RGB888
// 1 - MIPI_DSI_FMT_RGB666
// 2 - MIPI_DSI_FMT_RGB666_PACKED
// 3 - MIPI_DSI_FMT_RGB565
dsi,format = <0>;
Thank you for this information. I will recalculate the intended programmed DSI clk timings and provide you with feedback here.
In current summary, I am seeing the configuration as successful:
941AS SER [Internal PATGEN] --> FPD-Link --> 948 --> Display (successfully shows color bars - no flower screen)
Can you please confirm this so we may focus on SoC DSI TX --> 941AS DSI RX control path?
Thanks,
Miguel
1、941AS SER [Internal PATGEN] --> FPD-Link --> 948 --> Display (successfully shows color bars - no flower screen)
It's like this. It works
Hello,
clock-frequency = <148500000>;
hactive = <1920>;
vactive = <1080>;
hback-porch = <148>;
hfront-porch = <88>;
hsync-len = <44>;
vback-porch = <4>;
vfront-porch = <36>;
vsync-len = <5>;
pixelclk-active = <0>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <0>;
1、Continuous DSI CLK
2、Single DSI input, dual output
3、Not alternate line 3D mode
4、4 Number of DSI channels
5、DSI rate (Mbps): 290Mbps
With the PCLK of 148.5 MHz and 4 data lanes, I believe the DSI frequency should match the following:
fDSI = (fPCLK * 4) / 12 = 148.5 MHz * 3 = 445.5 MHz
DSI Datarate = fDSI x 2 = 891 Mbps
In this case, the TSKIP calculation would be
TSKIP_CNT = Round(65 * 0.4455 GHz - 5) = 24
Can you try configuring the SoC to output this 891 Mbps data rate per lane, and also change this Tskip value?
board.WriteI2C(serAddr, 0x40, 0x04) # DSI/DPHY Port 0 Registers board.WriteI2C(serAddr, 0x41, 0x05) # DPHY Skip timing board.WriteI2C(serAddr, 0x42, 0x30) # Set to decimal value 24
Since the clock is continuous, I am assuming that the SoC is outputting in Non-burst mode, please correct me if I am wrong - there is a different configuration needed entirely for Burst mode.
Best,
Miguel
1、It should be non-burst mode, due to the urgent development task, the temporary use of this set of hardware only replaces 941 and 948, replaced by other brands of serial chips can normally output 1920*1080 screen, and display normally, using TI 941/948 no matter how to adjust the screen is a display screen, but the color bar can be displayed normally. Contact the local FAE for support, they do not do offline support for us, so can only rely on online technical support
Hello,
Can you please refer me to the local FAE you have contacted? We will discuss with them about getting you dedicated support for this debug. I will continue supporting you here in the meantime.
Have any of the previous suggestions been implemented on the Source?
Best,
Miguel
We contacted colt-zhang, and fed back the problem to him at that time, asking him to do technical support. The reply from the FAE of TI said that we needed to read the manual by ourselves, and did not provide any support for our problem. After that, we could only look for support online all the time
Thank you for your patience.
I will put together a presentation recollecting all the previous data and next debug steps. I will relay this information to see if onsite support is possible, but I will also share this support debug flow here, allow me to put this guide together.
Best,
Miguel