This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
We are looking for a device which could bridge HDMI2.0 to DP++. Can we AC couple the TMDS181 output ?.
I believe typical TMDS output is open drain circuit, so generally could not be used with AC coupling.
Our considering setup is the following,
HDMI connector ---------> TMDS181 ---------> FPGA DP++ input
Best Regards,
Kawai
Hi Kawai-san,
DP++ is a feature of GPU(Source) it is not a feature of Display(Sink).
TMDS181 is an HDMI2.0 retimer, if you want to convert HDMI2.0 to DP you need a bridge, we don't have such devices.
Regards
Hello Moises-san and JMMN-san,
Thank you for your reply. First I had a wrong setup, required an AC coupling cap.
Referring JMMN-san's answer, I believe TMDS181 TMDS output circuit is open drain circuit, am I correct ?
i.e. without the pull up resistor at TMDS181 outputs, normal voltage swing level may not be able to pass through the AC coupling caps. I am thinking that with the following setup, correct TMDS181 output swing can be received at FPGA side with DC level cut.
x pull up with resistor
x |
HDMI connector ---------> TMDS181 --------> C --------> FPGA
Best Regards,
Kawai