This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401A-Q1: Are TFP401A-Q1 and TFP401 interchangable

Expert 1105 points

Part Number: TFP401A-Q1
Other Parts Discussed in Thread: TFP401, , TFP401A

Hello,

We are planning to use TFP401 in a project. Due to temperature requirements we need the automative version hence TFP401A-Q1

Are TFP401 and TFP401A interchangeable?

While reading through below E2E post, I got the impression that TFP401 and TFP401A are not the same in terms of outputted pixels?

https://e2e.ti.com/support/interface/digital_interface/f/130/t/556656

 I have read the hsync generation difference but don't think that it will cause a problem in our case.

Our input video is 800 x 600, 50Hz

thanks