Part Number: TUSB2077A
Other Parts Discussed in Thread: TPS2062
Hi,
I have a prototype design with the USB hub mentioned in the title, configured as self-powered, non-ganged.
My issue is that I can't get the downstream ports to work since the !PWRON-signals stay high all the time. I already noticed that the power switches TPS2066D have active high inputs, thus the current configuration doesn't work. I replaced them with TPS2062 devices, which incorporate an active low logic at the input pins. As this didn't solve the problem my idea was that the power-up sequence is wrong (the low signal at the reset pin at power-up is too short). I inspected this with a scope, a screen capture is attached. The schematic is attached as well.
If you could take a look at the schematic and the power-up timing I'd appreciate it.
Thanks in advance!
Tim