Part Number: DS125DF1610
Hello,
I'm having difficulty getting the DS125DF1610 to generate a PRBS output without an input waveform. I am trying to verify the egress and ingress transmission paths of our system.
My setup is the following: 1st DS125DF1610: TX (PRBS Gen) -> QSFP -> Loopback -> QSFP -> 2nd DS125DF1610: RX (PRBS Check).
The transmitter and receiver are different devices. We have a differential 25MHz clock connected to REF_CLK_P/N with daisy chained CLK_MON_P/N output.
At this point frequency accuracy isn't a priority.
I have tried forcing Signal Detect and CDR Lock, both independently and together.
I've also tried enabling EN_CLK_LOOPTHRU_LV. I just can't seem to get the outputs to turn on.
I have provided a Register Dump of the Transmitter DS125DF1610 below. Will worry about the RX device next. Thanks in advance.
Shared Registers
0x00 0x00
0x01 0x71
0x02 0x00
0x03 0x00
0x04 0x01
0x05 0x08
0x06 0x00
0x07 0x05
0x08 0x00
0x09 0x00
0x0a 0x00
0x0b 0x40
0x0c 0x00
0x0d 0x81
0x0e 0x00
0x0f 0xff
0x10 0xff
0x11 0x00
Global Registers
0xFC 0x00
0xFD 0x00
0xFE 0x03
0xFF 0x00
Channel Registers
0x00 0x00
0x01 0x00
0x02 0x00
0x03 0x00
0x04 0x01
0x05 0x01
0x06 0x01
0x07 0x01
0x08 0x60
0x09 0x20
0x0A 0x50
0x0B 0x6f
0x0C 0x08
0x0D 0xb4
0x0E 0x93
0x0F 0x69
0x10 0x3a
0x11 0x20
0x12 0xe0
0x13 0x90
0x14 0x00
0x15 0x13
0x16 0x7a
0x17 0x36
0x18 0x40
0x19 0x20
0x1A 0xa0
0x1B 0x03
0x1C 0x90
0x1D 0x00
0x1E 0x91
0x1F 0x55
0x20 0x00
0x21 0x00
0x22 0x00
0x23 0x40
0x24 0x40
0x25 0x00
0x26 0x00
0x27 0x00
0x28 0x00
0x29 0x00
0x2A 0x30
0x2B 0x0f
0x2C 0xf2
0x2D 0x07
0x2E 0x00
0x2F 0xb6
0x30 0x08
0x31 0x40
0x32 0x11
0x33 0x88
0x34 0xbf
0x35 0x1f
0x36 0x30
0x37 0x00
0x38 0x00
0x39 0x00
0x3A 0x00
0x3B 0x43
0x3C 0x20
0x3D 0x2a
0x3E 0x00
0x3F 0x41
0x40 0x00
0x41 0x01
0x42 0x04
0x43 0x10
0x44 0x40
0x45 0x08
0x46 0x02
0x47 0x80
0x48 0x03
0x49 0x0c
0x4A 0x30
0x4B 0x41
0x4C 0x50
0x4D 0xc0
0x4E 0x60
0x4F 0x90
0x50 0x88
0x51 0x82
0x52 0xa0
0x53 0x46
0x54 0x52
0x55 0x8c
0x56 0xb0
0x57 0xc8
0x58 0x57
0x59 0x5d
0x5A 0x69
0x5B 0x75
0x5C 0xd5
0x5D 0x99
0x5E 0x96
0x5F 0xa5
0x60 0x00
0x61 0x00
0x62 0x00
0x63 0x00
0x64 0x00
0x65 0x00
0x66 0x00
0x67 0x20
0x68 0x00
0x69 0x0a
0x6A 0x22
0x6B 0x40
0x6C 0x00
0x6D 0x00
0x6E 0x00
0x6F 0x00
0x70 0x03
0x71 0x20
0x72 0x00
0x73 0x00
0x74 0x00
0x75 0x00
0x76 0x22
0x77 0x1a
0x78 0x00
0x79 0x30
0x7A 0x00
0x7B 0x00
0x7C 0x00
0x7D 0x48
0x7E 0x13
0x7F 0x3a
0x80 0x00
0x81 0xe4
0x82 0x00
0x83 0x00
0x84 0x00
0x85 0x00
0x86 0x00
0x87 0x00
0x88 0x00
0x89 0x03
0x8A 0xdb
0x8B 0x00
0x8C 0x00
0x8D 0x02
0x8E 0x3c
0x8F 0x00
0x90 0x00
0x91 0x00
0x92 0x00
0x93 0x00
0x94 0x00
0x95 0x00
0x96 0x1C
0x97 0x00
0x98 0x0c
0x99 0x3f
0x9A 0x3f
0x9B 0x00