Part Number: MAX3232E
Hi Team,
Could you please help to double review the schematic design of MAX3232E as below? Left pins connected to on board MCU, and right pins connected to the RS232. And customer has few questions about the schematic design:
1, If the series resistors(R1221~R1224, R1217~R1220) on the input/output pin are needed? If yes, what's the recommend value? If not, the series resistance like below will worsen the signal performance?
2. If the pull up resistors on the R/1R2OUT pin are needed?
3. Customer found when add a pull up resistor at R1OUT pin connected to the other power rail, even device is powered off(VCC 0V), they measured flow backward voltage at VCC pin and RIN1 pin around 1V, like below picture 2. Can we explain the reason?
Thank you.