Part Number: TUSB321
Dear Team,
Please review my schematic and let me know if I am missing anything.
Mode : UFP
Current : 3A,5V
Thank you!
Regards
Mit shah
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB321
Dear Team,
Please review my schematic and let me know if I am missing anything.
Mode : UFP
Current : 3A,5V
Thank you!
Regards
Mit shah
Hi,
Since you are using TUSB321 in UFP mode, I recommend using OUT 1, OUT 2 and ID. To convene information to the AP or MCU. Since you are in a UFP only application then R2 is not necessary. This pin controls advertised current mode (only applied in DFP or DRP as host modes).
Hello Malik,
Thank you for your inputs.
I was confused in the out1,out2 pins but it is clear now.
Please find the updated schematic below:
Now I am taking out1,out2 and id pins in MCU so that we can detect the current mode.
My only question is if a PD enabled adapter is connected to type-C then can TUSB321 will handshake with it?
Or i have to use a PD controller.
I only need 5V@3A (15W).
Reagrds,
Mit
Hi Mit,
No in this case you do not have to have a PD controller. Please check the link below if you are unsure on when to choose a PD or CC controller. Yes, If a PD controller is connected over the CC line, CC negotiation will still occur but there will be no PD messaging after this.
Is there any more support needed for this issue? If so please reply with any relevant details so that I can further assist you. For now I will be marking this thread as "TI Thinks Resolved". If you have resolved your issue, please post the solution to the original problem/post for others with similar issues.