This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Connection of unused power switch

Part Number: TPS65987D

Hi team,

Can you help out with the following customer inquiry?

We only use one power switch of the device. According to the example circuit in the datasheet, the unused power switch (VBUS2, PP_HV2) is connected to GND.


However, the datasheet also contains the following contradictory statement:

Do pins VBUS1 and VBUS2 only have to be connected together if both power switches are used?
Since we are planning to have our prototype manufactured soon, a quick answer would be very helpful.

Thank you,

Franz