This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: Stability Issue link video FPD-LINK III

Part Number: DS90UB949-Q1
Other Parts Discussed in Thread: ALP

Hi,

I contact you because we are experiencing a curious problem in the use of the FPD-LINKIII link, in particular in the combination:

• DS90UB949TRGCTQ1 serializer
• DS90UB948TNKDRQ1 deserializer

The link is configured to work dual-lane.
In particular, we see that by connecting them together with a wiring of less than 30 cm in length, a transient occurs in which the video sent to the screen flickers and sometimes even disappears, and then stabilizes and no longer manifests the phenomenon. Using cables of longer length we never find the problem.

From a first analysis we see that the deserializer does not indicate an unlock of the video link and also electrically the link seems to operate in the correct operating parameters.
We would therefore like to have your support to understand what the causes of this behavior may be, and how to correctly direct the analysis.
For example:

• is there a length limit under which the link may not work properly?
• could the "transient" we see be due to the automatic channel equalization? In this case, in our system the registers that govern it are set to the default values. Could it be necessary to set them differently?


This problem affects products in production.

Please also write me in private if needed.

Thank you again for your availability and support.
Many Thanks,

Antonio F.