Part Number: AM26C31
Hi Team,
Currently are using AM26C31 for the design. There are several questions about the application of am26c31
1. As shown in the figure below, is the maximum driving capacity of am26c31 20mA? Since in ABS table, the maximum of output Io is 150mA
2. As shown in the figure below, what is the appropriate value of the impedance matching resistance in series on the differential output line? As I notice on datasheet, there is a guideline in 9.2.1 for 80 to 120ohm
3. As shown in the figure below, how to calculate the hardware filter bandwidth when RC is paralleled between differential output lines? If the design bandwidth is 1MHz, how appropriate is RC?