This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using IC TUSB1002A repeater board in cascade connection. I need to understand insertion losses to improve the signal integrity and also for the selection of equivalization setting based on our block diagram.
Thanks for the reply. I tried all the channel equalization setting range suggested for PCB 1& 2 for all the settings it worked. And what is the calculated insertion losses for PCB-1 and PCB-2 ?. And the reason for selecting VOD & gain for setting # 12 do you have any calculation reference example based on insertion losses selection (VID at 5 GHz = VOD x (10 -(Gv/20))?.
As you told it may change during USB compliance testing? Can you please suggest what can be done should we need to test eye diagram in hardware testing ? We dont have super speed signal testing
Hi,
Correct setting 12 for both PCBs. DC boost is set to +1 for both channels with 1200 mV VOD. This setting covers the most applications but may be changed during the tuning process/compliance testing.