Other Parts Discussed in Thread: ISO1228
Quickly find solutions to common questions about isolated interface devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Isolated Interfaces
| Digital Isolators | Isolated Interfaces | Opto-Emulators | |
I2C Isolators:
- [FAQ] Why is the logic LOW level output voltage, VOL1, up to 0.8V on Side 1 of the ISO1540 and ISO1541 bidirectional I2C isolators?
- [FAQ] ISO1640: Why are the maximum load capacitance and load current ratings for Side 1 of the ISO1640/ISO1641 less than Side 2?
- [FAQ] Can I connect two unidirectional channels on digital isolators to achieve a bidirectional channel for I2C communication?
- [FAQ] What are the recommended logic HIGH and LOW voltage levels that can be applied to the isolated I2C devices, ISO1540 and ISO1541?
- [FAQ] What is the current consumption of the isolated I2C devices, ISO1540 and ISO1541?
RS-485 Isolated Transceivers:
- [FAQ] How do you generate isolated power for an isolated RS-485 node?
- [FAQ] How do you configure a RS485 Full-duplex transceiver as Half-duplex?
- [FAQ] What kind of transient protection do you need with isolated RS-485 devices?
- [FAQ] What is the relationship between cable length and data rate for TI's isolated RS-485 transceivers?
- [FAQ] When is isolating an RS-485 bus necessary?
- [FAQ] What is the speed vs. length correlation for isolated RS-485?
Isolated Digital Inputs:
ISO121x
- [FAQ] How do you isolate multiple digital input channels with limited board space?
- [FAQ] How do you provide an LED status indicator with ISO121x digital input receiver devices?
- [FAQ] How do you set current limits and voltage thresholds in your system using digital input modules?
- [FAQ] What is sinking type and sourcing type inputs?
- [FAQ] How to set sinking type or sourcing type in ISO1228?
- [FAQ] Can ISO1228 Support Both Sink and Source Mode Operation at the Same Time?
- [FAQ] What is ISO1228's current limit feature? What is IEC 61131-2 type 1, 2 and 3 inputs?
- [FAQ] How does wire break detection work?
- [FAQ] How to achieve Type 2 in ISO1228?
- [FAQ] How do we set thresholds in ISO1228?
- [FAQ] How is Internal Surge Protection achieved in ISO1228?
- [FAQ] Can INx be Greater than AVCC? (Sink Mode)
- [FAQ] How to Enable Sink/Source Mode without Terminal/Component Changes?
Isolated USB:
- [FAQ] ISOUSB111: Can I use ISOUSB111 as a replacement device for ADuM3160 / ADuM4160?
- [FAQ] ISOUSB211: I would like to order ISOUSB111 or ISOUSB211 samples, but they are out of stock on TI website. Is there any other way I can still order these parts?
- [FAQ] ISOUSB211: What isolator do I use for a Class Compliant USB Audio Isolator?