This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LSF is not a logic buffer but a passive switch.
For input voltages below Vref_A, the LSF behaves like an analog switch. For input voltages above Vref_A, the switch is open, and the output voltage is created by the pull-up resistor.
Hey Mahima,
The LSF0204 can be used with I2C interfaces- however the device would require external pull up resistors and specific biasing requirements. For proper device operation see The Logic Minute Series as a reference.
The TXS0102 can also be used to support level shifting with I2C interfaces and differs from LSF0204 as the architecture includes internal pull up resistors and one-shot circuitry. Note that external pull-up resistors are not recommended for this device.
Regards,
Jack