This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Are you aware of any conditions such as supply noise or brownout condition that would cause the direction to swap from B->A to A->B erroneously given below schem?
Decaps are of course, placed close to device and solid ground pour is used.
Best
dimitri
Hi Dimitri,
Yes, noise or burnout issue could lead to faulty conditions on OE or DIR for directional changes i.e for example, a short to VCC on DIR may cause direction to swap from B->A to A->B erroneously. Additionally, a slow / floating input or noisy input may also cause DIR to pick up a high instead of low for A->B.
You may further confirm if any damages, i.e if issue is consistent with all other units / just 1 unit or if related to system environment, thanks.
Best Regards,
Michael.
Thank you Michael,
In this case, OE and DIR are both shorted to GND with copper so i would be surprised if they could float.
Additionally, a slow / floating input or noisy input may also cause DIR to pick up a high instead of low for A->B.
So for Slow inputs, what is the mechanism that would cause DIR to pick up HIGH? I would think that a Fast / sharp transient would be what would couple to DIR.
And could you recommend any mitigation for this case? E.g. RC Filter, 10k pulldowns on each pin, small cap like 100pF/220pF to ground? PWM frequency is only 500Hz so there is not any issue with attentuation.
Best
Dimitri
Hi Dimitri,
So for Slow inputs, what is the mechanism that would cause DIR to pick up HIGH? I would think that a Fast / sharp transient would be what would couple to DIR.
Please help see [FAQ] How does a slow or floating input affect a CMOS device? to help confirm if the expected waveforms for LOW observes similarities with the oscillation for HIGH as well i.e do you observe noise around 1/2 Vcc?
And could you recommend any mitigation for this case? E.g. RC Filter, 10k pulldowns on each pin, small cap like 100pF/220pF to ground? PWM frequency is only 500Hz so there is not any issue with attentuation.
If specific recommendation is needed, please further help clarify which case is precisely the concern i.e noise, slow / floating inputs, shorts or damages, etc, thanks.
Best Regards,
Michael.
Please help see [FAQ] How does a slow or floating input affect a CMOS device? to help confirm if the expected waveforms for LOW observes similarities with the oscillation for HIGH as well i.e do you observe noise around 1/2 Vcc?
Oh i see the concept , may be solved with schmitt trigger
thanks for the help, i will ask any further questions if i receive more info