This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVTH125: SN74LVTH125 Maximum operating supply current(ICC) during 3.3V LVTTL 50 ohm load drive

Part Number: SN74LVTH125

Tool/software:

Hi Team,

We are planning to use the SN74LVTH125 to drive the 1PPS signal output in our design. As per our design requirement 1PPS signal need to drive 50 Ohms load with <5ns rise time requirements.

So we planned short the four output signal and input signal to share the output load current.

What will be the maximum operating supply current(ICC) during 3.3V LVTTL 50 ohm load drive?

Regards,

Ramesh.