Part Number: TXB0104
Other Parts Discussed in Thread: TXU0104
Tool/software:
Hi,
I am using the TXB0104 in my design (schematic attached.
in my design VCCB is 5V and VCCA is 3.3V
- The input to VCCB is off / 24V fed to the pins via resistor split as shown in attached picture.(i,e: 44.2K and 10K to GND)
The issue is that i expected to get 4.42V and i get 1.5V ( I verified and the reason is the connection to the IC).
I tried also to alter the circuit and place on the input pin a p.d of 53.6K to GND and then find resistor so the overall divider will give me >3.25V (Vih min per datasheet)
1. I failed to find any combination to meet my needs.
2. my calculations assumed that maybe there is internal resistance in parallel to the 10K....i got ~4K)....and based on that tried to make divider to get correct Vi...but no success
3. why is it not that straight forward.
4. i also tried to change the device to TXS0104...with external P.U...and no success