This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have 4 UART's with Rx Tx that I want to multiplex to one Rx Tx pair.
The UART signal level is 1.8V.
Prefer I2C multiplex control to select which pair to pass through.
I have searched and can not find anything appropriate, can you help?
What about SN74LV4052A (with logic control, not I2C)?
Sure, it is an analog switch, so it simply connects the selected input with the output, the direction (for the analog switch) is irrelevant, signals can go in or out. Think of it as a mechanical switch, once closed, signals can cross it from any direction.
But, I remind you, it has TTL logic control, not I2C