Other Parts Discussed in Thread: SN74LVC1G14
Hi,
my customer would like to know what's the state of enable pin OE and input pin A when left unconnected. Will it be high or low or undetermined? Do we have a schematic to show the input structure?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
my customer would like to know what's the state of enable pin OE and input pin A when left unconnected. Will it be high or low or undetermined? Do we have a schematic to show the input structure?
When a CMOS input is left unconnected, this is referred to as "leaving the input floating" and is very bad for the device.
There's an FAQ on this topic here: [FAQ] How does a slow or floating input affect a CMOS device?
It also includes a schematic for a typical CMOS input.
Hi Howard,
To answer your questions directly:
1. How do I know if the device is CMOS, BiCMOS or bipolar?
This will typically be stated explicitly in the datasheet. For example, in the SN74LV4T125 datasheet, page 1:
SN74LV4T125 is a low-voltage CMOS buffer gate...
2. How do I know if the device have Schmitt-trigger input?
This is a little bit harder to answer. Typically, a Schmitt-trigger input device will directly state that. For example, the SN74LVC1G14's title is "SN74LVC1G14 Single Schmitt-Trigger Inverter"
This is not always the case, however. It's best too look in the electrical characteristics table to find the input threshold specifications. A standard CMOS device will only specify VIH and VIL, while a Schmitt-trigger input CMOS device will specify VT+, VT-, and ΔVT.