Hi,
We could have the following setup :
Driver/Receiver A <---------------> TXB0104 A <------------------> TXB0104 B <------------------------> Driver/receiver B
In this setup, Driver/Receiver A and driver/receiver B are for several seconds in a high impedance state after a power up. The TXB0104 are enabled and after a few seconds the drivers/receivers on both sides will be configured as one driver and one receiver.
The question is what is going on when both driver/receivers A and B are in high impedance ? What happens if for some reason the voltage level between Driver/receiver A and TXB0104A is equivalent to a logic high and the voltage level between Driver/receiver B and TXB0104B is equivalent to a logic low ? Will there be a conflict ?
Best regards,
JF Hasson