This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G08-Q1: SN74LVC2G08-Q1 - High and Low level Input thresholds

Part Number: SN74LVC2G08-Q1


Hi , 

We are using SN74LVC2G08-Q1 in our project application and I am trying to measure the high level and low level input thresholds. I am observing that VIH= 1.671V which is lesser than the minimum value (2V) mentioned in the datasheet and VIL = 1.225V which is higher than the maximum value (0.8V) mentioned in the datasheet . What could explain the deviation?