This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I can find an example of SBL for SD card boot in SDK, which uses FAT file system. So, we can just copy an image file into SD and can boot the system.
My question is whether or not we can boot the system from "OSPI Flash" in the same way with SD boot using the file system. If it is possible, I would like to know the relevant information or an idea about how to format the flash with FAT file system. Does TI flashing tool support this? I would appreciate it if you share how to put the image in the flash memory in this case, and the booting sequence.
Regards,
Moonil
Hi Moonil,
The answer is no, because the ROM bootloader will not boot load the SBL using file system, but using the address (0x0) for OSPI and EMMC. ROM bootloader does read SBL (tiboot3.bin) from file system on SD card.
Of course, the SBL_OSPI and SBL_EMMC can be changed for using the file system instead of the address for combined AppImage (app), but the current version of the SBL_OSPi and SBL_EMMC does not support the filesystem on neither OSPI nor EMMC.
Best regards,
Ming
Hi Ming,
Can you let me know if there is any plan to support the file system for SBL_OSPI?
And I wonder if we can use the file system for any memory type after bootup? for example, I also considered using SPI MRAM to write/read setting data through the filesystem during operation. Can we use file system for this case after system bootup?
Regards,
Moonil
Hi Ming,
Can you update the release schedule including the file system for NOR Flash and SBL_OSPI?
I think it can provide a convenient way to manage firmware images and their upgrade procedures, and also manage some system setting values on flash. It may require flash tools updated accordingly.
Best regards,
Moonil
Hi Moonil,
I have checked the MCU+ SDK release schedule. The file system support for SBL_OSPI and SBL_EMMC is not in the feature list of the 08.02.00 (scheduled for 2/28/2022). The schedule beyond 08.02.00 (2/28/2022) has not been determined yet.
SBL_NOR is not currently supported in the MCU+ SDK.
Best regards,
Ming