Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hello,
In the SPNU499c ref. manual, a note for the EDACEN bits of the FEDACCTRL1 register (Table 5-14) suggests that:
| Note: It is recommended to enable ECC in the Flash wrapper by writing 1010 to these bits before enabling ECC in the CPU. If ECC is enabled in the CPU, but not in the wrapper, the CPU will still check and correct single-bit ECC errors, and generate aborts on uncorrectable errors for the main Flash. However, the generation of ESM events, the capture of failing addresses and the detections and correction of errors in the OTP will be prevented |
In the application, we enable Auxiliary Control Register bit #25 as per spnu499c TRM para. 2.2.3.2, to enable ACTM ECC for the main flash array.
Does the above quoted text saying that the FEDACCTRL1->ECDACEN bits should be enabled by writing 0xA to it before enabling bit #25 of the Auxiliary Control Register?
Thank you for your helps.