This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How many days does it take for the AM24_DDR_Initialization_ECC_Disabled GEL script to complete? I am running it on the TMD2243GPEVM development board, and it has been running for over 18 hours now.
Hi Paul,
Use the SBL NULL is the recommended way to initialize the DDR. There is a catch though. The SBL NULL from MCU+ SDK of AM243x does not initialize the DDR. The SBL NULL from MCU+ SDK of AM64x does initialize the DDR. So download the latest MCU+ SDK AM64x and use the SBL_NULL from C:\ti\mcu_plus_sdk_am64x_08_01_00_36\tools\boot\sbl_prebuilt\am64x-evm\sbl_null.release.tiimage for OSPi flash write or SD card boot. It will do the DDR initialization for you. No need to use GEL file.
Best regards,
Ming
Hi Paul,
The AM243x 17x17 (on AM243x EVM) is the same as the AM64x (on AM64x EVM), plus the sbl_null.release.tiimage is actually runs on R5F_0_0 (which uses the 32 bit instructions), so it is perfectly OK to run the sbl_null.release.tiimage for AM64x on AM243x.
To try it quickly without write to your OSPI flash, you can use the SD card boot option. See AM64x MCU+ SDK: EVM Setup (ti.com) (SOC Initialization Using SD BOOT section) for details.
Best regards,
Ming
I put mcu_plus_sdk_am64x_08_01_00_36\tools\boot\sbl_prebuilt\am64x-evm\sbl_null.release.tiimage onto the SD card, and re-named it as tiboot3.bin
. I installed the SD card, change the switches to the SD boot setting, and powered the development board. I got the following messages on the terminal:
Starting NULL Bootloader ...
DMSC Firmware Version 21.9.0--v2021.09 (Terrific Llam
DMSC Firmware revision 0x15
DMSC ABI revision 3.1
INFO: Bootloader_runCpu:150: CPU r5f1-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:150: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:150: CPU m4f0-0 is initialized to 400000000 Hz !!!
INFO: Bootloader_runCpu:150: CPU a530-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:150: CPU a530-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:202: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:202: CPU r5f0-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runSelfCpu:219: All done, reseting self ...
I did not see any messages about DDR. Did it actually initialize the DDR?
Thanks for your help,
Paul
Hi Paul,
Yes, it does the DDR initialization. After the UART display the above message, you should be able to use the JTAG connect to the R5_0_0 core without using GEL file or launch.js. Once JTAG is connected to R5_0-0, you should be able to access the DDR (0x80000000) in the CCS Memory Browser. No need to run any GEL script.
Best regards,
Ming