Part Number: TM4C123AE6PM
Hi Team,
We would like to ask your help regarding our customer's inquiries below.
I am researching the TM4C123 Tiva C-Series microcontrollers for a new project and I have some questions.
1. When looking at the parts, I see there are multiple different types of USB peripheral. I just need to do the USB Device part. Is the Device part available with all of the USB peripherals? The TM4C123 part in the 64LQFP package with 64 or 128K flash part is our choice for a new product.
2. Same chip- has multiple types of USB peripheral. Do they all support Device mode?
3. Same chip- sometimes does not have a PWM-specific peripheral, but we think from the data sheets that we can set up a PWM pin with the standard timer module.
4. Same chip- has an implied change when more than 8 ADC pins are defined- it looks like that is the limit for one scan cycle.
5. Same chip- does not always advertise a "one-wire" capability. Is that something all of the Tiva-C chips support through the Peripheral Library?
6. Same chip- we think we can load a boot-loader on the chip that will manage two copies of our application- the "previous or current" version, and the "new or future" version, and that the bootloader can do this with an offboard part like a 265K FRAM chip, accepting the program over CAN.
Regards,
Danilo