Part Number: TM4C123AE6PM
Tool/software: Code Composer Studio
Hello,
I would like to use PC5 configured as GPIO_PC5_WT0CCP1 and capture the timer value of WTIMER0B on rising edge and automatically transfer the value on the timer to the uDMA every rising edge without have to reload or reset anything in software or use interrupts. Is this something that is possible? Currently I have the following code but I'm not sure that it is what I want or if I have it configured properly for what I would like to do. It looked like ping pong mode might be as close as I can get to continuous transfer but I just need to write the same value over and over no need for a buffer. The code listed below is only the code related to the GPIO, timer, and uDMA. Any assistance would be appreciated!!
HWREG(GPIO_PORTC_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
HWREG(GPIO_PORTC_BASE + GPIO_O_CR) = 0x01;
HWREG(GPIO_PORTC_BASE + GPIO_O_AFSEL) |= 1;
ROM_GPIOPinConfigure(GPIO_PC5_WT0CCP1);
ROM_GPIOPinTypeTimer(GPIO_PORTC_BASE, GPIO_PIN_5);//qmet_V5_00
// Clear the commit and lock registers just to be safe.
HWREG(GPIO_PORTC_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
HWREG(GPIO_PORTC_BASE + GPIO_O_CR) = 0x00;
HWREG(GPIO_PORTC_BASE + GPIO_O_LOCK) = 0;
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_TimerConfigure(WTIMER0_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_B_CAP_TIME_UP );
ROM_TimerControlEvent(WTIMER0_BASE,TIMER_B,TIMER_EVENT_POS_EDGE);
// enable uDMA must happen before configuration
ROM_uDMAEnable();
// Point at the control table to use for channel control structures.
ROM_uDMAControlBaseSet(pui8ControlTable);
// set up uDMA control settings to transfer data from WTIMER0B to location
ROM_uDMAChannelAttributeDisable(UDMA_CH11_WTIMER0B, UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST | UDMA_ATTR_HIGH_PRIORITY | UDMA_ATTR_REQMASK);
ROM_uDMAChannelControlSet(UDMA_CH11_WTIMER0B | UDMA_PRI_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_NONE | UDMA_DST_INC_NONE | UDMA_ARB_1);
ROM_uDMAChannelControlSet(UDMA_CH11_WTIMER0B | UDMA_ALT_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_NONE | UDMA_DST_INC_NONE | UDMA_ARB_1);
ROM_uDMAChannelTransferSet(UDMA_CH11_WTIMER0B | UDMA_PRI_SELECT, UDMA_MODE_PINGPONG, (void *)(WTIMER0_BASE + TIMER_B), &ulDutyTimer, sizeof(ulDutyTimer));
ROM_uDMAChannelTransferSet(UDMA_CH11_WTIMER0B | UDMA_ALT_SELECT, UDMA_MODE_PINGPONG, (void *)(WTIMER0_BASE + TIMER_B), &ulDutyTimer, sizeof(ulDutyTimer));
ROM_uDMAChannelAttributeEnable(UDMA_CH11_WTIMER0B, UDMA_ATTR_USEBURST);
// enable uDMA channel
ROM_uDMAChannelEnable(UDMA_CH11_WTIMER0B);
ROM_TimerIntEnable(WTIMER0_BASE,TIMER_CAPB_EVENT);
ROM_TimerEnable(WTIMER0_BASE, TIMER_B);