Hello,
I'm trying to control the dead band width of pwm in the code below, but the delay between the two LEDs lighting up doesn't seem to change no matter what I write in the function: PWMDeadBandEnable(PWM1_BASE, PWM_GEN_3, 10000, 10000); instead of 10000. Even if I write 0, or 65536.
Thank you for your time in advance.
#include <stdint.h>
#include <stdbool.h>
#include <math.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include <inc/hw_ints.h>
#include "driverlib/timer.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "driverlib/adc.h"
#include "driverlib/debug.h"
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_64|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN); //3,125 MHz
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
SysCtlPWMClockSet (SYSCTL_PWMDIV_64);
GPIOPinTypePWM (GPIO_PORTF_BASE, GPIO_PIN_2 | GPIO_PIN_3);
GPIOPinConfigure (GPIO_PF2_M1PWM6);
GPIOPinConfigure (GPIO_PF3_M1PWM7);
PWMGenConfigure (PWM1_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
PWMDeadBandEnable(PWM1_BASE, PWM_GEN_3, 10000, 10000);
PWMGenPeriodSet (PWM1_BASE, PWM_GEN_3 , 65535) ;
PWMPulseWidthSet (PWM1_BASE, PWM_OUT_6 ,32267) ;
PWMGenEnable (PWM1_BASE, PWM_GEN_3);
PWMOutputState (PWM1_BASE, PWM_OUT_6_BIT | PWM_OUT_7_BIT , true);
}