Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
I checked the example "OSPI Flash IO" in the MCU+ SDK to reference the clock frequency to OSPI Flash.
software-dl.ti.com/.../EXAMPLES_DRIVERS_OSPI_FLASH_IO.html
In the example, Flash and OSPI are configured by SysConfig and the OSPI clock seems to be set at 133 MHz / 4 = 33 MHz.
The S28HS512T supports up to 200 MHz clock in the datasheet.
AM243x supports up to 166 MHz (6.02 nsec) clock in DDR mode in the datasheet.
Are clock frequencies above 33 MHz validated for the TMDS243GPEVM?
Is there a detailed document for configuring Flash and OSPI by SysConfig?
Best regards,
Daisuke