This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我所用的开发板是,LP-MSPM0G3507,今天我想调试板子的时候,将错误的工程下载进了开发板里,里面的硬件配置都是不对的。下载完之后发现,已经无法用XDS110 USB连接开发板了。请问有没有方法能够补救回来。我希望能重置这个开发板。
The development board I used is LP-MSPM0G3507. When I tried to debug the board today, I downloaded the wrong project into the development board, and the hardware configuration in it was wrong. After downloading, it was found that it was no longer possible to connect the development board with XDS110 USB. Is there any way to remedy it. I hope i could reset this development board and delete the wrong project.
You can refer to this
Thank you so so much ! Now the problem has been solved.
I haven't tried the BSL solution. I just knocked and shake the damn board and then it fixed :) .
Maybe the plastic sleeve on the ping take effects. (I don't know)
Thank you Gao. 你很牛逼,谢谢。
Hell Gao!
This issue remains. It happened again. And I can't download the BSL_GUI_EXE.zip
It says "You do not have permission to view this directory or page."
This time 's error is that
Thank you.
You can find the GUI in the SDK
It is in the SDK …\mspm0_sdk_0_57_00_00_eng\tools\bsl\BSL_GUI_EXE
Hello Gary
When I try to connect the device. CCS will tell me that the device may in low power mode. Please try Force Reset.
And then I Click the Force Reset button, and after a while CCS will tell me to try mailbox Mass Erase.
And the Erase failed again. I think the reason why it can not be connected to PC is that my project has some problems.
I download the wrong project to the device and cause the problem.
Why I haven't asked you for several days. Because I have 2 MSPM0 board .
And now they both dead ...
I need help or I need a response that whether they are totally dead.
Sorry for using Chinese.
操作:
不断显示正在erase,但是不会成功。
图片太多,放在下面。
That seems in the case that the SWD and BSL be locked. The common case caused this is Non-main flash been erased with no data write into it. Do you enable the non-flash erase in CCS? Be careful to modify the non-main flash.
If SWD and BSL be locked both, you can just replace the MSPM0 device with a new one.
I have the same problem,It tips device enter low power mode,and can't connect xds110 download.
The early version devices do not support debug in low power mode but it can be recovered by BSL. But for the latest version of the device will not have this issue.
Is that the device really be in low power mode or just the CCS told you that the device may in low power mode.
The CCS always tells that the device is in low power mode and let you try force reset.