This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
By checking safety library source code, we don't find the test option "SRAM_PAR_ADDR_CTRL_SELF_TEST" is included by macro definition "_RM57Lx_".
Can you help confirm whether or not this test is suppported by RM57L843?
Thanks.
Hi Jagadish,
By reading TRM, it seems the test is supported by R5F device.
But why did you not implement it for RM57Lx device(RM57x also belongs to R5F devices)?
Thanks.
Hi Shenruming,
I mean i don't see any direct code for the "SRAM_PAR_ADDR_CTRL_SELF_TEST" in diagnostic library.
Actually ESM 3.15 is equivalent to the "SRAM_PAR_ADDR_CTRL_SELF_TEST"
To create this error you can refer below two threads:
--
Thanks & regards,
Jagadish.
Hi Jagadish,
What's the document you get the capture from? I don't find fault ESM 3.15 defined in sl_types.h.
Hi Shenruming,
What's the document you get the capture from?
The capture is from the datasheet.
I don't find fault ESM 3.15 defined in sl_types.h.
Yes, this is not implemented in safe TI diagnostic library.
--
Thanks & regards,
Jagadish.