Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
I Want to write a code for SPI protocol using driver function uint32 spiTransmitData(spiBASE_t *spi, spiDAT1_t *dataconfig_t, uint32 blocksize, uint16 * srcbuff); uint32 spiReceiveData(spiBASE_t *spi, spiDAT1_t *dataconfig_t, uint32 blocksize, uint16 * destbuff); just explain have use in code and build communication , explain the logic sir code i will try to built
regards
Jeeva